This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMS3655: Oscillation by Cff capacitor

Part Number: LMS3655


Dear all,

Our customer designed LMS3655 by WEBENCH.
However, the output oscillated.
The conditions are as follows;
 Input: 16.5 - 19 V
 Output: 5 V
 Iout : 4 A

Cff of this output is 1.2nF.
They delete this Cff, or less than 100pF, the oscillation is stop.

Is this output (Cff=1.2nF) a correct answer?

Best Regards,
PAN-M