This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61178: Cross reference

Part Number: TPS61178
Other Parts Discussed in Thread: TPS61088,

Hi,

I am trying to find the compatible part with MP3431, but the only solution I can find is TPS61178 & TPS61088,

is there any closer solution based on below requirements or compatible with MP3431? Thanks!

input operation voltage : 2V ~ 5V 

output operation voltage : 4.5V ~ 16 V (better if up to 20V) 

support about 30 W out output power 

programmable or settable input current limit 

Efficiency > 90% for 10 mA load at 4.5V output , Vin =3.6V 

Efficiency > 90% for 3A load at 9V , Vin = 3.6V 

Soft start 

Short circuit and over temperature protection 

Best Regards,

Patty Chuang