Hi,
I'm trying to determine the range of the max charging current of my circuit. I'm using a 604 Ohm ±1% as my R_ICHG.
By using 639 <= K_ICHG <= 715, I get:
Ichg_max = 715 / (604 * 0.99) = 1.196A
Ichg_min = 639 / (604 * 1.01) = 1.047A
Where does K_ICHG_ACC come into play? As its value is ±6%, should I add an additional 6% to Ichg_max and remove 6% from Ichg_min? What does it represent?
Thanks,
Fred