HI TI Team:
Customer BMS use BQ76940 to Balance&protect, Find not protect when debug ,The set status as follows:
1.The sampling resistor is connected in parallel with four 5mR resistors,calculated resistance value is 1.25mR
2.Set sys_ctrl1 0x04 register 0X18,sys_ctrl2 0x05 register 0X43, protect1 0x06 register 0X12,protect1 0x07 register 0X23,
3,After the register value is written in, when it is read out, the data can be mapped
4.Short circuit the load and read 0x00 register value as 0x80,this No SCD fault is detected.
5.Adjust the load so that the discharge current value is greater than the design value,read register 0x00 value is also 0x80,thisNo OCD fault is detected.
Please help me
Thanks
CQ.LV