This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
My customer is looking to add a 2nd source alternative to LM2665M6X/NOPB on the current design. We would be second sourcing ourselves in this case. So, question is - do we have a pin compatible alternative to our device, or something that would not require drastic board changes?
Thanks
Viktorija
Hi Viktorija,
Expert supporting this device is out of office. He will be back on the week of Jan. 6th.
Thanks,
Yinsong
Hi Viktorija,
To my knowledge, the pin-pin compatible device is LM2681 or LM2765, but their max load is 20mA. If the this is okay, then this can be considered as the 2nd source. Otherwise, I don't see another candidate.
Thanks,
Youhao