This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25892: Boost mode without host

Part Number: BQ25892

Dear Experts,

My charger using BQ25892 is running OK in charge mode. Now I want to use boost mode without host control.

Following d/s and my last question (link) , I checking:

1. BAT above BATLOWV <== OK 
2. VBUS less than BAT+VSLEEP (in sleep mode)  <== OK
3. Boost mode operation is enabled (OTG pin HIGH and OTG_CONFIG bit =1) <== OTG pin is pulled to HI
4. Voltage at TS (thermistor) pin is within range  <== OK
5. After 30 ms delay from boost mode enable

Based on Jeff answer (link), I think only need OTG pulled Hi or OTG_CONFIG bit =1.

But, in my design, when I pull OTG pin to HI and disconnect adapter, there is NO voltage present in VBUS pin. 

Can you give some insight please.

Thanks