This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62840: ESD diode for Input pins.

Part Number: TPS62840
Other Parts Discussed in Thread: TVS0500, ESD321, ESD351, TPD1E10B09-Q1

Hi,

We are using TPS62840 in our device to step down 6V to 3.1V. we are using 2 x 3Volt batteries, the batteries will be replaced by end-user therefore ESD diode is a requirement. According to datasheet maximum voltage at the input is 7V. ESD diodes used for GPIO have clamping voltage greater than maximum voltage rating. similarly, what is the suggested clamping voltage and breakdown voltage of ESD diode with operating voltage 6.5V(0.5V ceiling due to extra 0.1-0.2V of new batteries)?

Regards

Ashok