Dear Sir/Ms.
The customer confirmed that after the TPS23756 R_CLS was replaced with 1.5K ohm or 137 ohm, the Classification Current value would be the same as that in Datashhet.
But after using 137 ohm set to Class 2, 13W power can still be pumped from the PSE end. What other settings will affect the power load limitation? If the customer wants to limit Class 2, what are the methods?
Best Regards,
Kami Huang