This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV758P: question from customer

Part Number: TLV758P


hi, Team.

I've been asked by Customer as below.

part number : TLV75801PDBVR

request 1.

Could you try to have the line regulation with specific condition Customer will use to provide for customer?

the graph datasheet provided is different condition, it would be nice if we could provide it with specific customer requirement

Vout=1.5V、Iout=0.33A

input voltage changes from 2.8V ~ 6Vin

request 2.

Could you try to have the load regulation with specific condition Customer will use to provide for customer?

VIN=1.8V、Vout=1.5V、

Iout changes =0 ~ 0.33A

i understand that customer has to do this by themselves but just asking to see if we could provide or not.

please tell me to know we could support on this or not .