In order to making use of TPS61194 for the Backlight of Automobile. However there are some design issues about the TPS61194-Q1.
Would you like to help me figure out several factors that contribute to the above questions?
Q1: Why LCD screen blink both in the state of PWM<20% and in the state of PWM>70%?
RE: ?
Q2: What’s trigger the table phenomenon?
The LCD screen |
PC software |
|
|
Normal state (no blinking) |
Step 1、set PWM=75% from PWM=70% Step 2、set EN=0,then set EN=1(3.3V) |
|
|
Off normal state (blinking) |
Step 1、set EN=0,then set EN=1(3.3V) Step 2、set PWM=75% from PWM=70% |
|
|
|
|
|
|
RE: ?
Framework Diagram:
I need help filling out the question about TPS61194Q .pdf
PC software:
Backlight Unit: (LED:11S4P)
Schematic:
PCB: