Tool/software: WEBENCH® Design Tools
Hi,
We have designed the circuit to work as follows;
Input Voltage : 16-32V
Output voltage : 5V
Output Current : 20A
We are able to get a constant output voltage at no load. But when we add load to circuit it is only able to support upto 5A. When we increase the load above 5A the output voltage starts dropping.
Please give a solution for this issue. The circuit and details are attached with this email.
Thanks,
Sithara M