Hi,
I'm in the process of implementing the tps23754 as a modified copy of the TPS23754EVM-383 reference design. To finish my implementation, please help out with the following questions:
- I have no external power adapters. Can I then short VDD to VDD1?
- We wish to use the end product outdoor. Section 8.2.2.2 in the datasheet says "Outdoor transient levels or special applicatons require additional protection". Do you have recomendations or reference literature on such additional protection?
- Reference design slvu304c.pdf Figure 1: Does the active output rectification need a DC path or discharge of Q3 and Q5 gate pins?
Thanks,
Børge