Other Parts Discussed in Thread: BQSTUDIO, EV2400
Hello, I have a couple of questions related to current calibration.
1. What is the Capacity Gain? The technical reference manual explains what its value should be. But, there is no mention on how it is used. It seems like an irrelevant/unused parameter that stays in the manual as noise. The reference manual section "12.2.5.2 CC Gain/Capacity Gain Calibration" explains that the Capacity Gain = CC Gain x 298261.6178. However, When I do the current calibration using bqStudio, the Capacity gain is set to the same value as the CC Gain (which is the value of the shunt resistor in units of mOhm, not unitless ADC reading as explained in the reference manual). bqStudio and the reference manual contradicts. Which one should I believe? Maybe I am missing something.
2. Is there a way to set CC Gain directly on the bqStudio (+EV2400)? When I directly try to set it to any value less than 1 mOhm, the CC Gain value does not change. It stays as 1 (default value). Only after a current calibration, it is set properly. Are we supposed to do current calibration for every battery we produce? I was expecting that there should be a way to set CC Gain directly with the "golden file" (*.gg.csv) using bqStudio. Most of the parameters are set correctly using the (*.gg.csv) file, but CC Gain needs manual current calibration.
Best