This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR23630: About PFM and FPWM Mode

Part Number: LMR23630


Hello,

It's used with PWM when the load current is above half of the peak to peak inductor current ripple

Can I use LMR23630 with PFM and FPWM when the load current is above half of the peak to peak inductor current ripple or only can be used in DCM?

If yes, how can I set the mode?

Thank you