Hello,
I tested with LMR23630 EVM board and I could get the result like this when the Iout = 0.1A at the light load.
The minimum peak Inductor current to enter the PFM Mode is 300mA, so the yellow graph(Inductor current) shows PFM Mode control.
But, the yellow graph is also showing DCM(Discontinuous Conduction Mode).
What is the difference between DCM and PFM?
The Pink Graph is the voltage sw node. Why the voltage is ringing when LS switch is off?
Thank you