HI
We have a design that is using bq24075T as the charger.
There is a need to periodically check the voltage of the battery.
After we pull !CE high, took a ADC read and set !CE low (enable), we noticed that the charging does not resume.
The above observation is more prominent on batteries which are charged upto 90%, the none resumption is repeatable for the said battery.
Like to get some feedback:
1) Is this a normal operation of this charger?
2) Do you have any recommendation to suspend charging for ADC readout
INg