Hello,
In ticket https://e2e.ti.com/support/power-management/f/196/p/836278/3092463?tisearch=e2e-sitesearch&keymatch=TPS2492%20UVLO#3092463 it is recommended that "the UVLO threshold should be selected much lower than the operating Vin voltage", however how much lower is not specified. We are currently testing a system that operates at 24V with a 20.8V UVLO, is this sufficient headroom to avoid the issue described in the linked ticket? We can potentially lower this limit to 12V but would prefer to keep it at least above 17V.
Thanks