Other Parts Discussed in Thread: SN74LV244A, , TPS3808
Is it possible to directly connect a buffer (such as SN74LV244A) to the / MR pin of the TPS3808G01 and control ON / OFF without using MOSFETs?
Is it possible to control as shown in the figure below?
We have a circuit configuration that mounts a capacitor on the CT terminal and uses / RESET Delay Time (td).
For / RESET Delay Time (td), the following formula was used.
Calculated using CT = 180 [nF] of td (/ RESET Delay Time) in “7.6 Switching Characteristics”,
but “MIN = 0.7 [s], Typ = 1.2 [s], MAX = 1.7 [s]” There is description, but there is no calculation result.
Td(s)=CT(nF)/175 + 0.5×10^-3(s) = 180/175 + 0.5×10^-3(s) = 1.02907[s]
Please tell me how to calculate MIN = 0.7 [s], Typ = 1.2 [s], MAX = 1.7 [s].