This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R3-DEVICE-FW: Chem ID logging -disabling SOC measurement to avoid to trigger protections.

Part Number: BQ40Z50-R3-DEVICE-FW

Hello,

I am performing the Chem ID cycle for a new battery and the SOC measurement is completely wrong(normal due to the fact the learning cycle has not yet been performed).

When the SOC reach 100% the charging stop and I can't fully charge the battery.

I set RSOC =1 to force SOC at 99% but after  some time OC is set to 1 and the charging stop.

I had to reset a few time to decrease the SOC value to be able to fully charge.

Is there a way to disable the SOC measurement to perform the Chem ID logging without any protection?It's time consuming since each time the charging stop  I have to restart the logging.

Best regards,

Clement