Other Parts Discussed in Thread: BQ25882
Hello:
We are using the BQ25886 and using the TS pin as recommended in the datasheet to limit charge from 0*C to 60*C. We have
RT1 = 5.24kΩ
RT2 = 30.31kΩ
10k NTC
However we would also like to connect the TS pin to a microcontroller's ADC to measure the cell's temperature. However the voltage at said pin can swing over 3.3V at lower temperatures and damage our ADC.
I wanted to ask if there is a way you would recommend for us to be able to measure this pin on an MCU's ADC that can go up to 3.3V. We were thinking to use an opamp to scale the voltage into the MCU. Maybe I am missing an easier way.
On a similar note, assume if I have a simple opamp that consumes very low power. Could I power it from the REGN pin to perform this function? Would it not be advisable? This is for a very cost sensitive application so removing BOM components is desired.
Thank you for your time,
Eduardo Garcia