I can only find the typical value of VINTANA1 / VINTANA2 / VUSB3P1V output voltage in datasheet, what's the min/max value of them?
Thanks,
Antony
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I can only find the typical value of VINTANA1 / VINTANA2 / VUSB3P1V output voltage in datasheet, what's the min/max value of them?
Thanks,
Antony
Hi Antony,
These internal supplies are generated by the device and hence we have the typical values that you can check. These are not supposed to be used for any external purpose.
Why would you want the min/max values?
Regards,
Gandhar.
Hi Gandhar,
These LDO voltages need to be measured in the end-product production line, and be checked if they followed the spec or not. Therefore the ranges are requested. There's no special usage.
Thanks,
Antony