Other Parts Discussed in Thread: TPS2412
Hi Team,
Here’re some information about LM66100 application.
Circuit operation principles:
1. The circuit will include 2 independent power sources: external USB Bus and external power supply.
2. There are 3 possible configuration for power connection:
a) From USB Bus only
b) From external power supply only
c) From both USB Bus and external power supply
3. For both of 3 configurations the following protection types are required:
a) Reverse current protection for USB Bus
b) Reverse voltage (and maybe also current) protection for external power supply
4. My idea is to use 2 of LM66100 for each power source and connect between them for current sharing in case of both sources are connected
Please advise how 2 LM66100 should be connected upon the requirements listed above.
Thanks,
Shlomi