Other Parts Discussed in Thread: BQ25886, BQ25155, , BQ25887
Hello,
I have a 2s 7.4V 180mAh battery. I have come up with two ways of charging it
1. Using a switch to connect both cells in parallel and charging them using a 1s charger (similar to this guy https://42bots.com/resources/a-circuit-to-use-2-single-cell-li-po-li-on-batteries-in-series-and-charge-them-in-parallel/)
2. Using a 2s USB boost charging IC such as the BQ25886
Could anyone tell me which would be the more efficient approach out of these two?
Many thanks
Ken