This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90320: UCD90320 command line interface

Part Number: UCD90320

Hi,

I use Fusion Design online software to design UCD90320. 

Is software have command line interface?

Can you provide the document?

  • Hi

    Fusion GUI provided various command tool for individuals command. You can find those commands under bin folder of the installation.  You can also see the usage under doc folder. Moreover each command has help options

    Regards

    Yihe

  • I save .*tifsp file. But I can't find how to use command line interface to program.

    I don't want use Date Flash Script export file to program, because it cost about 4min. It too long to program.

    I want use USB Interface Adapter and command line interface. I think it can quick.

    Thinks. 

  • Hello

    As mentioned in the data sheet. system file is not recommended for production programming since the IO may not be under controlled state.

    You can use command line tool: Fusionconfigwrite.exe to download the data flash hex file

    Type FusionConfigwrite.exe  --help to get the usage.

    Regards

    Yihe