Other Parts Discussed in Thread: LM5060, INA301
Hi,
I'm analysing the potential use of the LM5060-Q1 in a truck application.
A 24V power converter output shall be disconnected from the load when its output reaches 20A continuously.
The customer's specs allows an overcurrent up to 22A during 100ms maximum, but classify the 20A set-point as Significant Characteristic (SC).
Unfortunely the LM5060-Q1 Pspice Model does take in account the thermal effects.
Considering that the ambient temperature will affect the MOSFET Rds and the LM5060-Q1 internal parameters (ISENSE, IOUT-EN etc),
could be possible to minimize the effect of these changes sum-up in the 20A set-point using resistors and thermistors associations
for RSENSE and ROUT for the automotive temperature range (-40ºC to +85ºC) and determine the current set-point's tolerances?
Please, could you give me a circuit and calculations as an example?
Thank you in advance for your support.