I'm designing a small tester to be used on our production line to test finished assemblies. What I'm looking for is maybe a part like the TPS2662 but allows the current limit to be changed. I want to make the initial power up of our DUT with a low current limit so if there's a power short we can catch it before damaging parts and then if this does not through a fault then we can change the limit and power up the DUT.
Our voltage is 24VDC and I'd like to start with something like 10mA and after power up we don't need more than ~600mA.
Maybe someone has a good idea or knows of a part that can do this?