This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65400: TPS65400 Status Byte Register: Bit 0

Part Number: TPS65400

Hello,

We have a design using the TPS65400 and are seeing an issue with both Switcher_1 and Switcher_2 operating.

When we were capturing the information from the TPS65400 status register it reports bit 0 (see image below).
This is an undocumented state. Could you please share more detail on this state?

Thank you, Keith

  • hi Keith,

    Application engineer, Lishuang Zhao, will check it and give feedback on Monday.

  • Hi Keith,

    1. For this byte, bit 0, we don't have any more detail about the fault or warning.Please capture and upload some waveform of Switcher 1 and Switcher 2, including Vin, Vout, SW, BST and PG.

    2. Do you use Switcher 3 and 4? Are they okay?

    3. Have you restarted to check the status? Because any bits set in the status register remain set even if the fault condition is removed or corrected. The fault bits in the status register remain set until one of the following occur: (Details can be checked in section 8.5.2.4 Fault Monitoring page 38 on datasheet.)

    • The device receives a CLEAR_FAULTS command.

    • A RESET signal is asserted by either issuing a SOFT_RESET or by asserting/deasserting the CE terminal.

    • Bias power is removed from the PMBus device.

    Thanks,

    Lishuang

  • Hello,
    Thank you for your help.  Here are answers to your questions:

    1. For this byte, bit 0, we don't have any more detail about the fault or warning. Please capture waveform of Switcher 1 and Switcher 2, including Vin, Vout, SW, BST and PG.
    [KK] I thought these were all in the document except the BST signal. PG was deasserted as the status was not good.

    2. Do you use Switcher 3 and 4? Are they okay?   
    [KK] These are not used

    3. Have you restarted to check the status? Because any bits set in the status register remain set even if the fault condition is removed or corrected. The fault bits in the status register remain set until one of the following occur: (Details can be checked in section 8.5.2.4 Fault Monitoring page 38 on datasheet.)
    [KK] Status is reset using CLEAR_FAULTS command. When the fault is only during start-up for a limited number of cycles the current overflow bit disappears. Otherwise it stays set.

    Thank you, Keith

  • Hi Keith,

    I have responded your questions through email, please check. 

    I will close this thread.

    Thanks,

    Lishuang

  • We found that these actions fixed the problem:

    1. lowering the switching frequency
    2. increasing input voltage
    3. delay in turning on the 2nd switcher 
  • Hi Keith,

    Thanks for your feedback. Glad to see your problem is fixed. 

    Thanks,

    Lishuang