Urgent!!
Hello Everyone,
I am trying to charge a Lithium Ion battery of 11.1V and 2.2 Ah. I am confused with the configuration of the Jumpers. I tried to debug but I couldn't charge the Battery can anyone help me out over here?
My jumper configurations are
JP1: 1-2
JP2: Short
JP3: 1-2 short
JP4: Short
JP5: 2-3 Short.
I had connected the Vin and PGND with 12V/2A adapter and at the output terminal +ve terminal of battery at VBAT and -ve terminal of battery at PGND. I kept the battery connected to the EVM for 2 Hours the battery wasnot charging. I have already burned out a EVM cant afford to loose one!
Anyone with some picture or video can help me out over here? The module I am using is BQ24133EVM-715-15V.
Thanks in advance.