This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5170EVM-BIDIR: The several buck mode issues

Part Number: LM5170EVM-BIDIR
Other Parts Discussed in Thread: LM5170

Hi team
I have several issues regarding the operation of the LM5170EVM-BIDIR, which I want to ask. I hope you can help and provide solutions to me.

I have followed the procedure to operate buck mode. For connection details can be seen in the picture.

My question.
1. Why is there no voltage on the 12 V side?
2. The voltage on J-17-pins 5 & 6 is 3.1 V and the current is 3.27 A. Why is the current at the pin high? Is it reasonable? The more I increase the voltage, the current will also increase.
3. Is the connection I have made correct for the buck mode operation?
4. My DC input is 33 V, how do I set the voltage to get 12 V?

I will wait for your reply. thank you