This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is there a high-speed DA, which is used in vGA applications, single-channel, 10-bit, requiring an interface level of 1.8V;

Other Parts Discussed in Thread: DAC3151, DAC5652, DAC900

Hi

Is there a high-speed DA, which is used in vGA applications, single-channel, 10-bit, requiring an interface level of 1.8V;

similar to adi's adv7123 and ADV7125, but the interface level is 1.8V;

Pls help recommended.

Thanks

Elsa