Other Parts Discussed in Thread: LMZ14201, LM2902
Tool/software: WEBENCH® Design Tools
I am using LM2776 switching regulator for -5V reference in my circuit. I needed 200 mA output current from this IC for the worst case scenario. So, I decided to use WEBENCH design tool for help.
I have given following inputs to the design tool:
input : +5V
Output : -5V
Current : 200 mA
Ambient temperature : 30°C
The desgin tool created one circuit and I followed it in my circuit design. But when the pcb is turned on, it gets heated as fast as possible and it's test point it delivers around +1.2V instead of negative output.
If I remove this circuit and turn on the board, other sections work flawlessly. When reconnect this circuit, it gets heated and affects it's power source. It's power source is LMZ14201 with +5V configuration. Without LM2776 circuit, LMZ14201 delivers 5V perfectly. If LM2776 is present, it will deliver only 1.96V (approximately).
Please tell me what might be the problem in the existing design. Used circuit is given below. Designed by Webench tool.
Thank you!