Other Parts Discussed in Thread: LM5170
Hello,
I am using the LM5170 controller in my project to control a bi-directional boost converter. Since I have not a dedicated voltage source connected at the HV port I have connected a constant 14V to the VIN pin of the chip. Also these 14 V are connected directly to the pin of the ramp generator network resistor where the VINX pin should be connected according to the datasheet (the other pin of the resistor is connected to RAMP pin of the TI chip). The board operates fine up to a certain current reference, however above that the current controlled seems to saturate, which I have noticed by probing the COMP pins of the chip. The voltage of these pins i.e. the Vea error signal is ~ 3V higher than the peak of the generated ramp (so it's higher than the peak ramp current even when considering the 1V offset). However the duty cycle of the MOSFET gate signals is not at its maximum value (as calculated from eq, 16). My question is how is it possible to have the controller saturated but the gate signal not?Is there an internal limit to the gate driver duty cycle when the controller saturates? Let me know if you require more information of how I setup the TI chip.
Thanks,
Stratos