Hi,
I'm looking at using the TPS61500 for a 10V, 0.3A TFT backlight design and I had some questions regarding the selection of the inductor.
1) There's no guideline for frequency selection vs. the inductance value. I understand it's a trade off between efficiency and component size but how do we calculate the correct value to use in the 4.7uH to 22uH suggested range for a specific frequency?
2) I assume that frequency selection is a continuous range and that values between those listed in table 2 of the datasheet can be used?
3) It's been recommended previously for buck regulator design, that ideally the inductor saturation current should be larger than the worst case current limit of the internal switching FET. Is this still the case for the boost topology used in the TS61500 and if not, what's a sufficient de-rating for the inductor saturation current? Is it possible to have large current transients or does the feedback resistor ensure that the current is kept within the designed limit?
4) There's no information in the datasheet for ensuring control loop stability - does this mean that operating in the recommended conditions with the recommended values is guaranteed to stable?
5) The datasheet recommends the compensation value being set to 470nF but the EVM appears to use a different value. Which is correct and is there a particular reason this is different?
Thanks