Other Parts Discussed in Thread: LMZ23610
Hi,
Is it possible to sync 2x LMZM33604 modules with one as a master and another as a slave using the SW pin as the output and the SYNC/MODE pin as the input? Datasheet says not to connect any components on the SW pins, but could this be a possible solution if I use a resistor-zener combination with a high enough resistance?
If this is possible, what should be the possible range of resistance I can use in series with a 4.5V Zener (eg not too low as to interfere with the SW pin and not too high to be loaded by the SYNC/MODE pin)? I am not able to find information on the input impedance of the SYNC/MODE pin but measuring with a DMM gives me around 600kΩ at steady state.
Thank you.
Best regards,
Saxon