We have found another problem with the Fusion GUI v1.8.25 (under Windows 7, 64-bit).
When two UCD9240s are connected in the same PMBus the GUI will not detect them (when only one is present, it will).
Fusion GUI 1.7 running on a Widows XP machine communicates to both UCDs without a problem.