Dear all,
i want to use the LMZM33602 to create a 16V supply from a 24V source. The 16V shall be the working voltage for a PWM dimmable LED string (5 LED's a 2.9V in series with a linear CC regulator). The CC Regulator should be dimmed with a PWM frequency of 1KHz. Will there be any issues (noise, heat, oscillation....) switching the load of the LMZM33602 with 1KHz? The LED string current will be 1.05A. System power output: 16V x 1.05A = 16.8W
Kind regards
Norbert