This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54302: Inductor Selection

Part Number: TPS54302


Hi,

According to TPS54302 data sheet, the minimum value of the output inductor(Lmin) is calculated with the equation 8 as follows.
If calculating Lmin under the following condition, 8.65uH will be given.

- Condition
Vout     = 1.8V
Vin(max) = 5.5V
Kind     = 0.35
Iout     = 1A
Fsw      = 400kHz
Lmin     = 8.65uH

On the other hand, 3.3uH will be given if using WEBENCH Power Designer. So, could you please tell me which result is correct?

Best regards,
Kato