Other Parts Discussed in Thread: BQ76PL455A-Q1
Hello,
I want to use BQ76PL455EVM with a F28379d Launch Board or Arduino Mega.
I have read the datasheet of BQ76PL455A-Q1 and there are some missing parts in my mind. Initially I just want to power it up and read some voltage values. So I will connect 3.3 VDC, GND pins, TX , RX pins to the related pins in uP and FAULT and WAKE up to the related GPIO pins.
(assume 6 cells are connected)
1. When I set HIGH the WAKEUP pin, does it wake up directly ? Should I set LOW after it WAKES UP (I have read something like that) ? If so, when ?
2. After WAKE it UP, should I configure its BAUDRATE, ID, number of CELL or does it makes automatically and starts to reading voltage values ? Do I need to configure it?
3. After configuration , how I can read voltage of cells (for example 1st cell ?
After these questions, I believe I can proceed on my own further.
Thanks.