This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ4050: The Remaining Capacity value stops counting before reaching the Full Charge Capacity

Part Number: BQ4050

The Remaining Capacity counter stops counting when it reaches 4058mAh and the SoC never reaches 100%.  I've cycled the battery many times and tried many different changes to the settings but it always gets stuck at 4058.  

the Full Charge Capacity of the battery is 4100mAh so the SoC stalls at 99%.  

I've configured the charge termination settings to:

Charge Term Taper Current = 250mA

Charge Term Voltage = 1mV

but the VCT never gets set nor does the Remaining Capacity counter reach 4100mAh.  The CEDV RC counter reaches 4100mAh though.

Here is the full log during a complete charge and the GG file.  The counter stops around line 3100 of the log but no status registers change.

0361.1_10_2020.gg.csv1_15_charge_full_log.xlsx