This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: maximum current can provide by TPS610994

Part Number: TPS61099
Other Parts Discussed in Thread: TPS61023

Hi everyone,

I have a wifi related application(MT7687FN), the maximum current is about 400mA when system starts up, and the average current is about <200mA, the voltage is 3.3v;

Two alkaline batteries connect directly to the board,but when the sysetem starts up it will reset sometimes because of  the output power is not enough, so i need a boost convert.

THE  1.5V<Vinput<3.1V, the output=3.3V, and the maximum current is 400mA, average current <200mA;

I want to know whether the TPS610994 is suitable for this application?