This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5150-Q1: Clarification for the equation - 38

Part Number: LM5150-Q1

Hi Texas,

In the Datasheet, LM5150-Q1 (SNVSAP6 –SEPTEMBER 2017).

I need the clarification on the Equation No. 38 (Pg. No. 28)

For calculating the Resr(max) for the output capacitor, Ccomp and Fcross is used.

As per example, 

Ccomp = 33nF

Fcross = 2.27K

Resr(max) = 23mohm but with calculation I got 212 ohm.

Moreover, in example Ccomp is used as 330uF instead of 33nF. Is this is a mistake or it is correct?

So, kindly confirm the equation with the unit to be used. Attached the datasheet screenshot for reference