This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54020: 3.3VIN with 5V bias

Part Number: TPS54020

Hi there,

Can TPS54020 support 3.3VIN with 5V bias?

Thanks.

  • Hi Jerry,

    Yes, this is supported.

    To add onto this, any sequence is ok for the TPS54020 but I would recommend having PVIN available before EN and/or VIN. This will help to ensure a smooth output ramp. If PVIN ramps up slower than the output ramp it could result in a non monotonic output ramp.

    Best Regards,
    Anthony