This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Team,
The LM3670MF-3.3/NOPB shows a Vout 3.3V fluctuation of +/-20mV at Vin: 5V, Iout=70mA.
However for this application it is required to have a much lower fluctuation (0.1% of Vout).
We are looking at the different options like:
-Is it possible to disable PFM for LM3670?
-Do we have a comparable LM36xx device without PFM? Would LM3671/LM3674 show a better stability on Vout?
-If not do we have a SOT-23 equivalent that would show a better stability in the output?
-If there are not P-2-P alternative what else can we propose? Iout max: 200mA, I typ: 90mA
Thanks in advance,
A.
Hi AnBer,
No, it is not possible to disable the PFM mode in LM3670. 0.1% output voltage accuracy is too tight for the device. we have TPS62200 device which is with SOT23 package but doesn't have FPWM mode. If the package is not a major requirement than there are some devices with FPWM mode. So, I would suggest you look at the link for your require device: http://www.ti.com/power-management/overview.html
Best regards,
Tanvee
Hi Tanvee,
Thanks for the answer.
Looking at alternatives you suggested in SOT-23 I saw:
http://www.ti.com/power-management/non-isolated-dc-dc-switching-regulators/step-down-buck/buck-converter-integrated-switch/products.html#p238min=1.5;4.5&p238max=5.5;6&p634min=-17;3.3&p634max=3.3;92&p451max=0.3;0.9&p236typ=0.00006;0.146&p212max=76.92307692307692;100&sort=p1130;asc
with Forced PWM but in SOT-23-THIN
TPS62561
TPS62240
Without Forced PWM in SOT-23:
TPS62200, TPS62203
TPS62260
-Any other options you would advise for 0.1% accuracy output at the specs specificied in my original post?
-Is the 0.1% accuracy output something that can be simulated on Webench?
-It does not seem we provide Webench sim for TPS62200, TPS62203. Is it planned?
Also only the PSPICE/TINA-TI transient model is provided.
Thanks in advance,
A.
Hi,
There is no device with 0.1% voltage accuracy. PSPICE or TINA model gives all information that can be achieved from the WEBENCH model. Currently, there is no planning for WEBENCH model.
Best regards,
Tanvee
Hi,
I am closing the thread as the discussion is ongoing through the e-mail.
Best regards,
Tanvee