Hi Experts,
Currently, i am working for PIR and Smoke sensor with ESP8266,i have my own PIR(IRA-S210ST01) design using an LM324 amplifier it connect with LM1117 power supply here i have faced the issue with ESP8266 wifi disconnect automatically that's why i choose BOOSTXL-TLV8544 evaluation board then my demo module working fine now. so i decided to use BOOSTXL-TLV8544 PIR schematic for PIR design i need some clarification for my below doubts,
this thread shows my previous problem about to why i chose TLV8544 amplifier https://e2e.ti.com/support/amplifiers/f/14/p/867310/3221664#3221664
1. i have changed the PIR sensor, i am going to use IRA-S210ST01 instead of IRS-B210ST01 with the same BOOSTXL-TLV8544PIR schematic if the sensor alteration makes any problem here or not.
2. i have designed my demo module with LM2596 regulator but that makes a lot of noise in output so i can't get constant output from my BOOSTXL-TLV8544PIR evaluation board then i have changed LM117 now that is working fine, but i want to add Non-ionized( IR& Photo diode-based) Smoke sensor with RE46C191 from Microchip because Ti does not have any IC like this, then i need to design fixed power supply for this design (3.3V, and >2A), here i am little confused to choose correct linear regulator for this design so kindly help to find low-cost liner regulator for my requirements.
regards
kannannatesh