I use BQ25886 to charge a 2cell 7.4V 2500mah battery. The setting as below :
ILIM = 2.36A , RILIM = 470R
ICHG = 0.98A , RICHG = 3K9
VBAT = 8.4V , RVBAT = 180K
VBUS = 6V 2.5A , OTG DISABLE , D+ & D- SHORT TOGETHER
Why the charging current is only 250mA ? Please verify the attached scematic having any mistake.
Best regards
KC So