Other Parts Discussed in Thread: LM5155
Hello All,
I am working with a client that requires the following:
input voltage: 3 - 18V
Output voltage: 2Kv
Output current 0.5mA
Output voltage ripple: <1%
I am looking at using the LM51551, but following the application note SNVA866, not only have a found multiple errors in this application note, but it only works for CCM and I need to run in DCM. Im choosing DCM due too the low power requirement and keeping the magnetic's low.
I am looking at running multiple secondary stages in series to achieve the voltage requires, this works fine in simulation, with other controllers and free running. But there doesn't seem to be much guidance for designing a step up flyback in DCM for the LM51551.
any help will be much appreciated.