Other Parts Discussed in Thread: TEST2
I measured my battey charge/discharge for chemistry ID.
My battery is 4S1P(14.8V) / 4800mAh.
I measured twice as below.
[Test1] -> Cell manufacture standard charge/discharge
0.2C(960mA) charging / 0.02C(96mA) stop charging and 2 hour resting.
0.2C discharging and 5 hour resting.
[Test2] -> TI example
0.1C(480mA) charging / 0.05C(mA) stop charging and 2 hour resting.
0.1C discharging and 5 hour resting.
We tested different current with the same pack, and the results are different.
Test1 result is 1359 and Test2 result is 1327.
Is it right result? and which is best one?
And what is max DOD error and %?
For ID1327, max DOD error is 0.85, and % is 0.12 I don't know the meaning of this.
Please teach me.
And also I will attach two kinds of test data. Please review it.
4800mAh_0.2C.zip is Test1.
4800mAh_0.1C.zip is Test2.