This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3697: LM3697 in 3*12 application

Part Number: LM3697

Hi Team,

In 3*12 application, (Led 3.06V@23mA), Vf will be 36.72V

1. What's the efficiency at 3*12 application? I only see 3*7 and 2*10 in datasheet.

2. Do you think 36.72V will be a risk if set the OVP to 40V?

3. Do you think Internal 1A Mosfet could support this? 

Thanks.

Penn