Hello,
We would like to have below functionality for battery pack BMS with bq78350:
1. Wake-up/Turn battery pack BMS/SMBus ON/OFF using a host-controlled latching ON/OFF switch (Can this be done using GPIO, KEYIN/PRES ?)
2. Perform SMBus SHA-1 authentication. If battery is authenticated by host uC, turn ON main battery pack output (CHG/DSCG FETs). Else turn OFF main battery pack output (FETs).
3. Host micro-controller for latching ON/OFF circuit and for SMBus communication to be powered by battery @ (3.3V/5V ~100s mA) ( using isolated DC-DC or GPIOs if possible).
Please let us know the correct procedure & required BMS interfaces (GPIO, KEYIN/PRES, isolated DC-DC) to implement the above functionality.
If you are able to provide a reference schematic/circuit diagram with bq78350 to implement the above functionality, it would be much appreciated.
Thank you very much.
Kailash