This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27520-G4: BQ27520-G4

Part Number: BQ27520-G4

We would like to know internal process of bq27520-G4 to detects the battery voltage when the battery connection is unstable and a sag occurs

In the reference manual of “SLUUA35”,  current value is described like that.

-Return the average current for 1 second to section 2.11,
-Section 2.18 states that the instantaneous current is returned every 128 ms.

But no description for voltage value.

Could you inform us of the process of  the battery voltage detection,  when the battery connection is unstable and a sag occurs